Assess the Safety Integrity Level (SIL) via a Layer of Protection Analysis (LOPA)

This topic describes how to assess the SIL level for an Instrumented Function using a LOPA.

Steps

  1. Access the Instrumented Function for which you want to assess the SIL value.
  2. In the workspace, select the SIL Assessment tab.

    The SIL Assessment section appears. The Assessment Details tab is selected by default.

    The SIL Assessment section

  3. In the lower-right corner of the Assessment Details subsection, select Add Assessment, and then select LOPA Internal.

    A blank LOPA Assessment datasheet appears.

    LOPA Assessment datasheet

  4. As needed, enter values in the available fields.

    Note: In the Linked LOPA ID field, you can only link LOPA records that are in Complete state.

  5. In the upper-right corner of the datasheet, select .

    The LOPA Assessment is saved, and the SIL level for the Instrumented Function is assessed using LOPA.

Results

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.