This topic describes attributes of the State Configuration that is defined for the SIL Analysis family in the baseline GE Digital APM database.
The following baseline states are defined in the GE Digital APM application:
The following baseline operations are defined in theGE Digital APM application:
These baseline states and operations are reserved, which means you cannot modify or remove them. You can, however, add your own states and operations to the state configuration.
The following flow diagram illustrates the State Configuration for the SIL Analysis family. In this image, a box represents a state, and an arrow represents an operation. The state to which an arrow points represents a successor state.
By default, the MI SIS Administrator and MI SIS Engineer State Configuration roles are assigned to all states in the SIL analysis state configuration. You can assign State Configuration roles to any state. In addition, for each state, the Require a specific user to be assigned to a state check box is selected.
Copyright © 2018 General Electric Company. All rights reserved.