The first time that you use Rounds on the Handheld Windows Mobile Device, you will need to retrieve the query parameters for the Download query from GE Digital. When you do so, the parameter values that are configured for the Download query prompts will be selected in lists that correspond with these prompts. You will need to use these parameters to download Routes.
The following instructions assume that you have specified the Download query on the Specify Download Settings screen.
Steps
Select Sync Data.
The following screen appears.
Select Sync.
The Synchronizer screen appears, displaying the progress of the download process.
After the Routes are downloaded to the Windows Mobile Device, the screen refreshes and displays a message indicating that the Sync is finished.
Select Close.
Fields appear that correspond with the query prompts for the Download query. At this point, you can download Routes to the Windows Mobile Device.
Copyright © 2018 General Electric Company. All rights reserved.