The log file contains information about events that have occurred on the Windows Mobile Device while you were using the GE Digital APM. In some cases, these events produce errors, which are also recorded in the log. For each event, you will see the following information:
For example, consider the following entry:
08/24/2009 15:10:42|Info|Creating Schema for Application||
From this entry, you can see that:
When an event produces an error, the log entry also contains the error information. For example, consider the following entry:
07/09/2009 15:21:42|Error|There was a problem synchronizing.|TargetInvocationExceptionSystem.Reflection.TargetInvocationException: TargetInvocationException...
Note: The error would continue, but the ellipsis has been added to the documentation to shorten the example.
From this entry, you can see that:
Copyright © 2018 General Electric Company. All rights reserved.