On the Home screen within the Rounds application, you can access the Specify Download Settings screen. This screen contains the following options:
If you want to use a different query, you must specify that query on the Specify Download Settings screen. Your changes are saved automatically.
Note: Before you can download Routes from GE Digital APM to the Windows Mobile Device for the first time, you will need to retrieve the parameters for the Download query.
Delete All Data: Select Delete All Data to delete all the readings and recommendations that are currently stored on the device. Delete All Data is disabled if no readings or recommendations are currently stored on the Windows Mobile Device.
At the bottom of the screen, Close button appears. This button closes the Specify Download Settings screen and then displays the Home screen.
The following image shows the Specify Download Settings screen.
In this image, you can see that the Delete All Data button is disabled (i.e., the text is gray). This means that there are currently no readings or recommendations stored on the Windows Mobile Device.
Copyright © 2018 General Electric Company. All rights reserved.