Update Checkpoints with Changes from the Source Template

If you modify the contents of a Measurement Location Template or Lubrication Requirement Template that was used to create a checkpoint (i.e., Measurement Location or Lubrication Requirement, respectively), you may want to update the corresponding checkpoints with the changes you made to the source template to keep them synchronized.

Steps

  1. Access the Templates section.
  2. In the list of templates, select the row containing the template whose corresponding checkpoints you want to update, and then select Update Existing Checkpoints.

    The Update Existing Checkpoints page for the selected template appears, displaying a list of the checkpoint records that are based on the template. The values in the checkpoint records that are different from the template, and thus will be updated to match the template, are highlighted.

  3. In the first column, select the rows for the records that you want to update with the changes from the source template.

    Hint: You can select the check box in the column heading to select all the rows.

  4. Select Update.

    The selected checkpoints are updated with the changes from the source template, and the Update Existing Checkpoint window appears, displaying a list of the checkpoints that were updated.

  1. Select to close the window.

    The Update Existing Checkpoints page displays the updated values for the checkpoints.

Copyright © 2018 General Electric Company. All rights reserved.