Interpret Reading Records

When you upload data to GE Digital APM, one Reading record is created for every reading value that was saved to the mobile device. The following table list the values that are populated in fields in Reading records after you upload data to GE Digital APM.

Field

Value

Action Taken

The value that was selected in the Action Taken cell on the Readings - Detail screen for the Measurement Location to which this Reading record is linked.

Asset ID

The value in the Asset ID field of the Measurement Location record to which the Reading record is linked.

Comment

The text that was entered in the Description cell on the Readings - Detail screen for the Measurement Location to which this Reading record is linked.

Reading Taken By

The name of the Security User who was logged on to Operator Rounds when the reading value was entered.

Reading Taken Date

The date the reading value was saved on the device.

Reading Value Character

The reading value if it is a character reading.

Note: This field is enabled only for character readings.

Reading Value Numeric

The reading value if it is a numeric reading.

Note: This field is enabled only for numeric readings.

Status

One of the following combinations of the ID and Description of the System Codes stored in the Reading Status System Code Table:

  • C (Completed)
  • I (Ignored)
  • NC (Non-compliant)

This value Indicates the compliance status for the reading.

Unit of Measure

The unit of measure associated with the reading.

Note: This field is enabled only for numeric readings.

Copyright © 2018 General Electric Company. All rights reserved.