Checkpoint Task Records

Checkpoint Task records store details on the schedule on which a checkpoint should be executed. This topic provides an alphabetical list and description of the fields that exist for the Checkpoint Task family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Last Date

Date

The date and time on which the last reading was recorded for this checkpoint.

This field is populated automatically after a Reading is created and linked to the Measurement Location to which the Checkpoint Task is linked, with the value in the Reading Taken Date field of the Reading.

Next Date

Date The date and time on which the next reading for this checkpoint becomes due. This field is populated automatically based on the values in the Schedule field and the Last Date field. If the Last Date field is empty, the value in the Next Date field is calculated as the next date and time that meets the defined schedule after the current date and time.
Non-compliance Date Date The date and time after which the reading will be considered non-compliant.

This field is populated automatically based on the values in the Schedule and the Next Date fields.

By Default, Non-Compliance Date value is populated as: Next Date Value + Non Compliance Date Interval (in days). If Non Compliance Date Interval is absent, then Next Compliance Date value is populated as: Next Date + Schedule Interval.

Non-Complinace Date Interval Numeric Its is the Non Compliance Date Interval (in days) added to Next Date to get the Non-Compliance Date.

This field is not populated automatically.

If Non Compliance Date Interval is absent, then Next Compliance Date value is populated as: Next Date + Schedule Interval.

Non-Compliance Next Check Date Date It is the date after which the Checkpoint is checked again for Compliance.

By Default, Non-Compliance Next Check Date value is = Non-Compliance Date

Schedule

Character The schedule by which you want to take readings for this checkpoint. This field contains an ellipsis button that you can select to access the Edit Schedule window, where you can define the schedule for the associated checkpoint.

Task ID

Character The ID of the Checkpoint Task. This field is populated automatically with a value in the format CP-<n>, where <n> is a number representing the number of Checkpoint Tasks that have been initiated (even if they were not actually saved). You can change the value, if needed.

Copyright © 2018 General Electric Company. All rights reserved.