Using the Node Pin Board pane, you can use the drag-and-drop method to move one or more locations, or Conditions from the Route to the Node Pin Board pane, and then later move them to new Checkpoints or remove them from the Route.
Checkpoints or Conditions on the Node Pin Board pane include any child Checkpoints or Conditions that are linked to the parent node.
You will not be able to drag and drop an item until the dark blue insertion marker appears under the node where the item will be dropped.
A Checkpoint that contains Conditions and subsequent Checkpoints can be dragged and dropped as a single entity. However, if you want to drag two top-level Checkpoints, you have to drag and drop each one separately.
When a Condition is deleted from the Route, the Checkpoints and Conditions that were successors to that Condition will be moved to the Node Pin Board pane.
You cannot drag and drop an Equipment or Functional Location to the Node Pin Board pane. However, if you remove an asset group from the Route, the associated Checkpoints, including any related conditions and subsequent Checkpoints, will be moved to the Node Pin Board