A Measurement Location Template can be used as the basis for creating multiple Measurement Locations. Measurement Location Templates store the details of the checkpoint template, which can be used to create Measurement Locations in a Route.
Measurement Location Template records can be successors to Checkpoint Condition records, which represent conditional logic that can be applied to the checkpoints. After a Template Group containing conditions is applied to a Route, the Measurement Locations that are created as successors within a condition will appear to the user only if the defined condition is satisfied.
Copyright © 2018 General Electric Company. All rights reserved.