RCA Hypothesis records store basic information about root cause of a failure event. The following table provides an alphabetical list and description of the fields that exist for the RCA Hypothesis family and appear by default on the RCA Hypothesis datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field Caption | Data Type | Description | Behavior and Usage |
---|---|---|---|
Confidence Factor | Character | A value that indicates the probability that the hypothesis is true. |
You can choose from the following values:
If you select a value in this field, the value that you select will appear in brackets to the right of the hypothesis name in the Logic Tree. |
Description | Text | A detailed description of the hypothesis. |
You can define this value manually when you create the RCA Hypothesis. |
ID | Character | The ID for the Hypothesis. |
This field is automatically populated and is disabled. |
Label |
Character | A description of the hypothesis as you want it to appear on the Logic Tree. |
You can define this value manually when you create the RCA Hypothesis. |
State | Character | The state of the Hypothesis node. |
You can choose from the following states:
This field is set to Hypothesis by default. |
Copyright © 2018 General Electric Company. All rights reserved.