When you create an RCA Preserve Item, the type of data that you
want a member of the Root Cause Analysis Team to collect is identified by one
of the following categories, known as the 5 P's:
- People: Indicates
that human witnesses should be questioned about the incident. Witnesses
might include the person who is responsible for the maintenance of
the piece of equipment or location associated with the failure event,
the operator, or even the stock room attendant.
- Parts: Indicates
that physical pieces of the equipment should be collected (i.e., the
broken pieces). This may also include collecting a functional piece
of equipment to test against the broken one.
- Paper: Indicates
that any data or information that exists about the piece of equipment
or location should be gathered. This could include recent performance
reports, schedules, GE Digital APM data, specifications, and so on.
- Position:
Indicates that the environment in which the piece of equipment or
location exists should be documented and considered. This could include,
for example, the temperature of the room at the time of the incident
or the proximity of one piece of equipment or location to another.
- Paradigms:
Indicates that any trends or common assumptions about the cause of
the incident should be considered. The intent of noting these paradigms
is to remove this assumption from the investigation (i.e., remove
any bias from the analysis).
You can select one of the 5 P's on the RCA Preserve records datasheet, in the Data Category box.