Criticality Calculator RBI Component records store information about the component on which you will perform an RBI
This topic provides an alphabetical list and description of the fields that exist for the Criticality Calculator RBI Components family. The information in the table reflects the baseline state and behavior of these fields. If the component type is Exchanger Bundle, then, for each field on the RBI Component, there are two fields on the datasheet - one for the channel, and the other for the shell.
The following families are enabled for site filtering, which means that the records in these families can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Criticality Calculator RBI Components
Field |
Data Type |
Description |
Behavior and Usage |
||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
The ID Section |
|||||||||||||||||||
Component |
Character |
Identifies the RBI Component. |
This field is disabled and populated automatically with a value in the following format: RBICOMP-<Equipment>-<Component Type>-<Number> ...where:
|
||||||||||||||||
Component Comments |
Text |
Comments about the component. |
None |
||||||||||||||||
Component Date in Service |
Date |
The date on which the component was first put into service. |
You can use the Calendar feature to select the date. |
||||||||||||||||
Component Description |
Character |
A description used to identify the Component. |
None |
||||||||||||||||
Component Status |
Character |
Indicates whether a component is active or inactive. |
This field is disabled and populated automatically with the value Active. |
||||||||||||||||
Component Type |
Character |
Identifies which part of the asset the component represents. |
The value in this field must be stored in the Criticality Item Type field in one of the Equipment Types records delivered in the GE Digital APM database. This field is disabled and populated automatically. |
||||||||||||||||
Equipment |
Character |
Identifies the asset. |
This field is populated automatically. |
||||||||||||||||
Equipment Family |
Character |
Identifies the asset family. |
This field is disabled and populated automatically. |
||||||||||||||||
Functional Location |
Character |
Identifies the Functional Location of the asset. |
This field is disabled and populated automatically. |
||||||||||||||||
Operating and Process Section |
|||||||||||||||||||
Area Humidity |
Character |
A value based on the geographical location in which the asset is operated. |
|
||||||||||||||||
Calculated Inventory |
Numeric |
A calculated value based on process fluid properties and dimensions of the component. |
This field is disabled and populated automatically. This value is derived from asset dimensions that have been entered in the system instead of an estimated volume. |
||||||||||||||||
Detection Time |
Numeric |
The time, in minutes, that is required to detect loss of containment. |
None |
||||||||||||||||
Fluid Valid for 581 Analysis |
Boolean |
Indicates whether the process fluid is valid for an RBI 581 Risk Analysis. |
This check box is disabled and selected if the fluid that you have selected in the Process Fluid field is valid for RBI 581. If this check box is cleared, and you perform an RBI 581 Risk Analysis, you will not be able to calculate the analysis. |
||||||||||||||||
Foundation Type | Character | If the component is a storage tank, then specify the foundation type of the tank. |
The value in this field is used to calculate an analysis if the component type is Storage Tank. This field contains the description of all the System Codes in the FOUNDATION TYPES System Code Table. You can choose from the following baseline values:
|
||||||||||||||||
Initial Fluid Phase |
Character |
The phase that the representative fluid is in while under containment in current operating conditions. |
This field contains the description of all the System Codes in the FLUID TYPES System Code Table. You can choose from the following baseline values:
|
||||||||||||||||
Inventory |
Numeric |
The volume of the asset that could potentially be released in the event of a failure. |
The value in this field is used to populate the Inventory Component Mass field in the RBI Consequence Evaluation that is linked to an analysis performed on this component. |
||||||||||||||||
Inventory Group | Character |
The name of the inventory group to which the component is linked. |
This field is disabled and blank. |
||||||||||||||||
Isolation Time |
Numeric |
The time, in minutes, that is required to isolate loss of containment. |
None |
||||||||||||||||
|
Numeric |
The internal pressure of the asset under normal operating conditions. It is measured in pounds per square inch gauge. |
The value in this field is used to populate the Operating Pressure field in the associated analysis. |
||||||||||||||||
|
Numeric |
The temperature of the asset under normal operating conditions. It is measured in degrees Fahrenheit. |
The value in this field is used to populate the Operating Temperature field in the associated analysis. |
||||||||||||||||
Percent Toxic |
Numeric |
The amount of toxic substances by volume in the process stream. |
This field is enabled only if the Toxic Mixture check box is selected. |
||||||||||||||||
Process Fluid |
Character |
The fluid that represents or makes up the greatest volume of the asset. In some cases, the fluid that represents the greatest cause of failure may be selected. IMPORTANT: If you are going to perform an RBI Criticality Analysis, you must select a fluid that is valid for RBI 580. Similarly, if you are going to perform an RBI 581 Risk Analysis, you must select a fluid that is valid for RBI 581.
|
The value in this field must be stored in the Fluid field in one of the Representative Fluids records in the GE Digital APM database. |
||||||||||||||||
Toxic Fluid |
Character |
The fluid that represents or makes up the greatest toxic volume of the asset. In some cases, the fluid that contributes to the greatest Consequence of Failure (CoF) may be selected. |
This field is enabled only if the Toxic Mixture check box is selected. The value in this field must be stored in the Process Fluid field in one of the Representative Fluids records delivered in the GE Digital APM baseline database. |
||||||||||||||||
Toxic Fluid Valid for 581 Analysis | Boolean |
Indicates whether the toxic fluid is valid for an RBI 581 Risk Analysis. |
This check box is disabled and selected if the fluid that you have selected in the Toxic Model field is valid for RBI 581. |
||||||||||||||||
Toxic Mixture |
Boolean |
Indicates whether or not the process stream contains toxic substances. |
If you select this check box, the Toxic Fluid and Percent Fluid boxes are enabled. |
||||||||||||||||
Design Details Section |
|||||||||||||||||||
Code Year |
Character |
The year in which the design code that corresponds to the component was defined. |
The value in this field must be stored in the Code Year field in the GE Digital APM Reference Table that corresponds to the value in the Stress Lookup Table field in the RBI Component record. The value in this field is used to populate the Code Year field on the datasheet of the associated analysis. |
||||||||||||||||
Construction Code | Character | The code to which the component was originally constructed. |
The value in this field is used to populate the Construction Code field on the datasheet of the associated analysis. |
||||||||||||||||
Design Pressure |
Numeric |
The pressure at which the component is designed to operate. It is measured in pounds per square inch gauge. |
The value in this field is used to populate the Design Pressure field in the associated analysis. Tip: This value is provided by the manufacturer of the component. You can find it on the nameplate or the UI Form. |
||||||||||||||||
Design Temperature |
Numeric |
The temperature at which the component is designed to operate. It is measured in degrees Fahrenheit. |
The value in this field is used to populate the Design Temperature field in the associated analysis. Tip: This value is provided by the manufacturer of the component. You can find it on the nameplate or the UI Form. |
||||||||||||||||
Inside Diameter |
Numeric |
The measurement of the inner diameter of a circular or cylindrical asset, in inches. |
The value in this field is used to:
|
||||||||||||||||
Insulated? |
Boolean |
Indicates whether or not the component is insulated. |
If you select or clear this check box, the Insulated check box on the datasheet of an associated RBI Analysis is selected or cleared accordingly. |
||||||||||||||||
Insulation Type |
Character |
Identifies the insulating material used in the component. |
This field is enabled only if the Insulated? check box is selected. The value in this field is used to populate the Insulation Type field on an associated RBI This field must contain one of the following values:
|
||||||||||||||||
Is Entry Possible? |
Boolean |
Indicates whether it is possible to physically enter an asset for the purposes of performing an inspection. |
This field contains the description of all the System Codes in the MI_YES_NO System Code Table. You can choose from the following baseline values:
|
||||||||||||||||
Length |
Numeric |
The total length, in inches, of an asset measured in a straight line from head seam to head seam. |
This value is used to |
||||||||||||||||
Material Grade |
Character |
Identifies the grade of the material of the component provided by the manufacturer. You can find it on the nameplate or the U1 Form. |
The value in this field must be stored in the Material Grade field in the GE Digital APM Reference Table that corresponds with the value the Stress Lookup Table field in the RBI Component. The value in this field is used to populate the Material Grade field on the datasheet of the associated analysis. |
||||||||||||||||
Material Spec |
Character |
Identifies the material of the component that is provided by the manufacturer. You can find it on the nameplate or the U1 Form. |
The value in this field must be stored in the Material Spec field in the GE Digital APM Reference Table that corresponds with the value the Stress Lookup Table field in the RBI Component. The value in this field is used to populate the Material Spec field on the datasheet of the associated analysis. |
||||||||||||||||
Nominal Thickness |
Numeric |
An estimated or measured thickness used as the starting point for thickness based Remaining Life calculations. |
The value in this field is used to populate the Nominal Thickness field on the datasheet of an associated RBI |
||||||||||||||||
PWHT |
Boolean |
Indicates whether or not Post Weld Heat Treatment (PWHT) has been performed to relieve residual stresses from the construction of the asset. |
|||||||||||||||||
Stress Lookup Table |
Character |
Identifies the type of asset being assessed so that the appropriate design codes are used. |
This field contains the description of all the System Codes in the MI_STRESS_LOOKUP_TABLE System Code Table. You can choose from the following baseline values:
The value in this field is used to populate the Stress Lookup Table field on the datasheet of the associated analysis. |
||||||||||||||||
Weld Joint Efficiency |
Numeric |
Indicates the type of inspection used to ensure the quality of welds and the type of weld joints used during construction. |
This field is used to populate the This field must contain one of the following values:
|
||||||||||||||||
Corrosion Data Section |
|||||||||||||||||||
Corrosion Type |
Character |
The type of corrosion to which equipment is susceptible. |
You can specify a value for this field using the datasheet. |
||||||||||||||||
Corrosive Product |
Character |
Identifies the elements in the process stream that are responsible for the most aggressive corrosion. |
None |
||||||||||||||||
Estimated External Corrosion Rate |
Numeric |
The rate of external degradation given by the subject matter expert during the corrosion study. This value is used in the absence of quality data from the field. |
The value in this field is used to populate the Estimated Rate field on an associated |
||||||||||||||||
Estimated Internal Corrosion Rate |
Numeric |
The rate of internal degradation provided by the subject matter expert during the corrosion study. This value is used in the absence of quality data from the field. |
The value in this field is used to populate the Estimated Rate field on an associated |
||||||||||||||||
Internal Corrosion Type |
Character |
Used in inspection planning to drive different activities for localized and general thinning mechanisms. |
This field contains the descriptions of all the System Codes in the CORROSION TYPES System Code Table. You can choose from the following baseline values:
|
||||||||||||||||
Measured External Corrosion Rate |
Numeric |
The corrosion rate, in inches per year, identified by Ultrasonic Thickness or Profile Radiography in the field. |
None |
||||||||||||||||
Predictable Corr. Location |
Boolean |
Indicates whether or not it is known where the most aggressive corrosion is happening in the asset. |
None | ||||||||||||||||
Predictable Int. Corr. Location |
Boolean |
Indicates whether or not it is known where the most aggressive internal corrosion is happening in the asset. |
None | ||||||||||||||||
Source of Calculated Corrosion Rate |
Character |
The source of the Thickness Monitoring Calculated Corrosion Rate. |
The value in this field is used while integrating this module with Thickness Monitoring. This field contains the descriptions of all the System Codes in the MI_RBI_CALC_CORRO_SRC System Code Table. You can choose from the following baseline values:
The following table provides the behavior of the Controlling Corrosion Rate, Short Term Corrosion Rate, and Long Term Corrosion Rate fields in the associated RBI 581 Thinning and Lining Evaluation or Criticality Int. Corr. Deg. Mech. Eval. based on your selection in this field.
|
Copyright © 2018 General Electric Company. All rights reserved.