Finalize Risk of Multiple RBI Criticality Analyses

This topic describes how to finalize risk of all the analyses that are linked to multiple Assets or Corrosion Loops. You cannot finalize risk of multiple analyses that belong to the same component. You can finalize risk of only the analyses that are calculated and are in the Created state.

Steps

  1. Access theRisk Based Inspection Overview page, and then select the Assets tab.

    -or-

    Access the Unit Summary workspace of the Process Unit that is linked to the Corrosion Loops.

  2. In the Assets section, select the check box for each asset containing analyses for which you want to finalize risk.

    -or-

    Select the check box for each Corrosion Loop containing analyses for which you want to finalize risk.

    The button is enabled.

  3. Select .

    The Finalize Analysis Risk window appears, displaying only the analyses that are calculated and are in the Created state.

  4. Select the check box for each analysis for which you want to finalize risk.

    The Finalize Risk button is enabled.

  5. Select Finalize Risk.

    The selected analyses are moved to the Risk Completed state.

  6. Select Close.

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.