When you promote an asset to Asset Strategy Management (ASM), a Risk is created in ASM for each Degradation Mechanisms record (DM) in active RBI
The following table provides a list of fields on the Risk datasheet that are populated from the DM or the associated RBI
This Risk field: |
...is populated with: | ...from the following associated records: |
---|---|---|
Name |
A value in the following format: <Equipment Description> ~ <Degradation Mechanism> If there is no value in the Equipment Description field, then the value in the Equipment Type field is used. |
RBI |
Description |
A value in the following format: <Equipment Description> ~ <Degradation Mechanism> If there is no value in the Equipment Description field, then the value in the Equipment Type field is used. |
RBI |
Failure Mode | The value in the Degradation Mechanism field | DM |
Maintainable Item | A value in the following format: <RBI Component Entity ID> ~ <Equipment Description or Equipment Type> | RBI |
Failure Cause | The value in the Degradation Mechanism field | DM |
Unmitigated Financial Risk | The value in the Unmitigated Financial Risk Rank field | DM |
Risk Basis | The value Risk Based Inspection | None |
Copyright © 2018 General Electric Company. All rights reserved.