About Values Mapped to Action

When you promote an asset to Asset Strategy Management (ASM), an Action is created in ASM for each RBI Recommendation in active RBI Criticality Analyses. This Action contains the details of the Recommendation.

The following table provides a list of the fields on an Action datasheet that are populated from the RBI Recommendation.

This Action field:

...is populated with:
Action Basis The value RBI Recommendation.
Action Source The value RBI.
Action Task Type The value in the Task Type field.
Action Basis The value in the Action Type field.
Cost The value in the Estimated Cost field.
Cost Basis The value in the Estimated Cost Basis field.
Description <Recommendation Inspection Scope> ~ <Recommendation Basis>
Interval

The least value among the following:

  • The value in the Interval field in the RBI Recommendation
  • The value in the RBI Half-Life field in the associated Degradation Mechanism Evaluation
  • The value in the TM Half-Life field in the associated Asset Corrosion Analysis.
  • Time Based Inspection Settings

Interval Basis

The value of the Interval Basis that corresponds to the Interval field (only if the value in the Override Interval field in the Task is set to False).

Interval Units The value Months.
Name <Damage Mechanism> ~ <Task Type>
Nonrecurring The value in the NonRecurring? field.
Shutdown Required The value in the Asset Shutdown Required? field.

Copyright © 2018 General Electric Company. All rights reserved.