The RBI
In RBI, State Configuration is used in the following families:
Notice that a pink background surrounds several states in the diagram.
When an RBI
Additionally, in the diagram, you can see blue lines and black lines.
Blue lines represent operations that are performed automatically when another RBI
Black lines represent operations that you can perform manually.
Note: While the
preceding image includes the Reject operation and the Rejected state,
this state and operation are not valid in the RBI workflow and are, therefore,
colored gray in the image. While they exist in the baseline State Configuration,
if you try to reject an RBI
Initial State
The Created state is the initial state of all new RBI
Datasheet Configuration
By default, states and operations will appear on the datasheet when
you are viewing an RBI
Reserved States and Operations
The following tables state whether or not the baseline states and operations are reserved. You cannot remove or modify reserved states or operations. You can, however, add your own states and operations to the State Assignment.
States and Operations | |
---|---|
States | Is Reserved? |
Approved |
Yes |
Accepted by ASM |
Yes |
Archived |
Yes |
Created |
No |
Implemented |
Yes |
Pending Approval |
Yes |
Re-Evaluating |
Yes |
Rejected |
No |
Risk Completed |
Yes |
Operations | Is Reserved? |
Archive (all Archive operations) |
Yes |
Implement |
No |
Finalize Risk |
No |
Reevaluate |
No |
Approve |
No |
Reject |
No |
Reimplement |
No |
Promote to ASM | Yes |
Submit for Approval | No |
State Assignment Roles
By default, no State Assignment
Roles are assigned to any state in the RBI
The following table outlines the actions that you can perform on an RBI
Analysis State | Calculation is Allowed? | Analysis Can Be Deleted? | Analysis Fields Can Be Modified? | RBI Degradation Mechanisms Can Be Added or Deleted? | What-If Analyses Can Be Created? | RBI Recommendations Can Be Created? |
---|---|---|---|---|---|---|
Created |
Yes |
Yes |
Yes |
Yes |
Yes |
No |
Risk Completed |
No |
No |
No |
No |
Yes |
Yes |
Pending Approval |
No |
No |
No |
No |
No |
No |
Approved |
No |
No |
No |
No |
No |
No |
Implemented |
No |
No |
No |
No |
No |
No |
Archived |
No |
No |
No |
No |
No |
No |
Rejected |
No |
No |
No |
No |
No |
No |
Re-Evaluating |
No |
No |
No |
No |
No |
No |
Accepted by ASM |
No |
No |
No |
No |
No |
No |
If an RBI
Copyright © 2018 General Electric Company. All rights reserved.