When you create and save an analysis that is based on a query or dataset, the GE Digital APM system saves the data that exists at the time of creation. When you open an existing analysis, changes made to the underlying query or dataset since the analysis was created will not be reflected automatically.
Note: If the query or dataset has been deleted or renamed, when you try to open an associated analysis, an error message will appear and the data will not be refreshed.
If you want to refresh an analysis to reflect changes to the underlying query or dataset or to load new data that has been added since the analysis was last saved (e.g., the analysis is based on a query that retrieves failures for a piece of equipment or location, and a new failure record has been added to the database), you will need to reload the analysis manually after opening it. When you reload the data, any manual changes made to the analysis data set will be deleted.
Note: Reloading analysis data resets the analysis period only if it is based on the analysis data. Start Dates and End Dates that have been set explicitly will not be overwritten.
Steps
In the left pane, select the Production Data tab.
The Production Data workspace appears.
In the upper-right corner of the workspace, select Analysis Data, and then select Reload Data.
A confirmation message appears, asking you to confirm that you want to overwrite the current data with the data stored in the database.
Note: For an analysis based on manually-entered data, you will receive the following error message:
There is no source data to reload since the analysis is based on manually entered data.
Select Yes.
The analysis is updated to reflect the data currently stored in the query or dataset.
Note: If you are reloading analysis data that is based on a query and an index out of range error message appears, there is an error in the query. You should modify the query or recreate the analysis to reload the correct data.
Copyright © 2018 General Electric Company. All rights reserved.