You can use the Reliability Growth Data window to modify the data in any enabled field. This allows you to correct errors in the data or adjust data as needed. Only certain fields in the Reliability Growth Data window can be modified. Fields that contain calculations by the GE Digital APM system are disabled.
Steps
In the left pane, select the Cumulative <Measurement> Plot tab.
The Cumulative <Measurement> Plot appears in the workspace.
Note: You can also modify data for a plot via the Mean Time Between <Measurement> Plot, and <Failures> Rate Plot tabs.
In the upper-right corner of the workspace, select Analysis Data, and then select Edit Data.
The Reliability Growth Data window appears, displaying the data associated with the selected Probability Distribution Analysis.
As needed, modify the data in any enabled field, and then select OK.
The analysis is updated to reflect any changes that you made.
Select Finish.
The analysis is updated to reflect any changes that you made.
Results
Copyright © 2018 General Electric Company. All rights reserved.