Import a Reliability Distribution Analysis

You can create new Asset elements by importing existing Reliability Distribution Analyses into a Diagram. You can import one or more analyses in a single operation. One Asset element will be created for each record that you import, and a new System Asset record will be created to store information for that element. Fields from the Reliability Distribution record will be mapped to the System Asset record, as described in the Results section.

This topic describes how to add an element by importing a Reliability Distribution Analysis to a Diagram. You can also add an element directly to a diagram.

Steps

  1. Access the Diagram within which you want to import a Reliability Distribution Analysis.
  2. In the Import section, select .

    A list of available Reliability Distribution Analyses appears.

    Import

  3. Select check box to the left of the Reliability Distribution Analysis that you want to import.

    Tip: You can select more than one Reliability Distribution Analysis.

  4. In the upper-right corner, select Import.

    A new Asset element is added to the Diagram for each selected Reliability Distribution Analysis.

    Asset

Results

When you import an existing Reliability Distribution record into the Diagram, a new System Asset record is created, and information from the imported record is mapped to the System Asset record. Information is also mapped to System Risk and Distribution records, which are created when a record is imported and linked to the System Asset record.

The following table contains the values that are imported from fields in records from a Distribution Analysis and the System Analysis record and field to which they are mapped. All other values in System Analysis records are populated automatically with default values.

Note: If you import an asset and import the Reliability Distribution Analysis associated with that asset, all of the fields in the following table will be mapped except the Analysis ID field will not be mapped to the Name field in the System Asset record.

Reliability Distribution Analysis Record Reliability Growth Record Field System Analysis Record System Analysis Record Field Notes
Reliability Distribution Analysis ID System Asset Name None
Reliability Distribution Analysis ID System Risk Name None
Reliability Distribution Failures Without Replacement System Risk Failures Without Replacement None
Distribution Short Description Distribution Short Description This value is mapped from the TTF and TTR Distribution records that are linked to the Reliability Distribution record to the corresponding TTF and TTR Distribution records that are linked to the System Risk records.
Distribution Distribution Type Distribution Distribution Type This value is mapped from the TTF and TTR Distribution records that are linked to the Reliability Distribution record to the corresponding TTF and TTR Distribution records that are linked to the System Risk records.
Distribution Units Distribution Units This value is mapped from the TTF and TTR Distribution records that are linked to the Reliability Distribution record to the corresponding TTF and TTR Distribution records that are linked to the System Risk records.
Exponential MTBF Exponential MTBF This value is mapped from the TTF and TTR Distribution records with a Distribution Type of Exponential that are linked to the Reliability Distribution record to the TTF and TTR Distribution records with a Distribution Type of Exponential that are linked to the System Risk records.
Lognormal

Mu

Sigma

Gamma

Lognormal

Mu

Sigma

Gamma

This value is mapped from the TTF and TTR Distribution records with a Distribution Type of Lognormal that are linked to the Reliability Distribution record to the TTF and TTR Distribution records with a Distribution Type of Lognormal that are linked to the System Risk records.
Normal

Mean

Standard Deviation

Normal

Mean

Standard Deviation

This value is mapped from the TTF and TTR Distribution records with a Distribution Type of Normal that are linked to the Reliability Distribution record to the TTF and TTR Distribution records with a Distribution Type of Normal that are linked to the System Risk records.
Weibull

Beta

Eta

Gamma

Weibull

Beta

Eta

Gamma

This value is mapped from the TTF and TTR Distribution records with a Distribution Type of Weibull that are linked to the Reliability Distribution record to the TTF and TTR Distribution records with a Distribution Type of Weibull that are linked to the System Risk records.

Copyright © 2018 General Electric Company. All rights reserved.