After you add elements to a Diagram, you must connect the elements to create the Diagram. Depending on the structure of the system for which you are creating a Diagram, you will want to connect elements to each other in a series or parallel to one another.
Steps
In the design canvas, select the circle on the element from which you want to initiate the connection, and then drag your pointer to the required destination (i.e., the circle on the element that will serve as the end of the connection). An arrow is drawn automatically in the direction that you drag your pointer.
When your pointer touches the port of the required destination, release the pointer to set the connection.
The connection will be completed automatically.
Copyright © 2018 General Electric Company. All rights reserved.