The Minimum Production Output is the value used to replace all zeros and negative numbers in the Production Analysis. When you create a new analysis, if the source data contains zeros or negative numbers, you will be prompted to specify a Minimum Production Output value. You will also be prompted to set the Minimum Production Output value if you modify or reload the data to contain zeros and negative numbers in an existing analysis that did not previously contain zeros or negative numbers. You can use the following instructions to modify the value that is currently saved with the analysis.
Steps
Access the Production Analysis whose Minimum Production Output you want to change.
In the left pane, select the Production Data tab.
The Production Data workspace appears.
In the upper-right corner of the workspace, select Analysis Tasks, and then select Minimum Production Output.
The Set Minimum Production Output window appears. By default, the Minimum Production Output value is set to the value that was selected when the analysis was last saved.
In the Minimum Production Output box, enter the value that you want to use to replace zeros and negative numbers, and then select OK.
The Production Analysis is generated with the new Minimum Production Output value.
Copyright © 2018 General Electric Company. All rights reserved.