The baseline GE Digital APM database includes the Spares Analysis Report, which you can use to view a summary of Spares Analysis results.
The Spares Analysis Report is built from the following Catalog items:
Throughout this documentation, we refer to the main report, the subreports, and the supporting queries collectively as the Spares Analysis Report.
The Analysis Properties section of the Spares Analysis Report displays information that is stored in the Spares Analysis record. The name of the analysis, which is stored in the Analysis ID field of the Spares Analysis record, is displayed in blue at the top of the Analysis Properties section.
The following table lists each item in the Analysis Properties section and the corresponding Spares Analysis record field whose data is displayed in the report.
Report Item | Record Field(s) |
---|---|
Analysis Properties | |
Description | Short Description |
Start Date | Analysis Start Date |
End Date | Analysis End Date |
Currency | Number |
Simulation Options | |
Iteration | Iteration Number |
Random Seed | Random Seed |
Events Logged | Enable Event Log |
Each Spare Analysis record can be linked to multiple Spare records. In the Spares Analysis report, a Spare Properties section will appear for each Spare record that is linked to the Spare Analysis record. The name of the spare, which is stored in the Spare ID field of the Spare record, is displayed in blue at the top of each Spare Properties section.
The following table lists each item in the Spare Properties section and the corresponding Spares Analysis record field whose data is displayed in the report.
Report Item | Record Field(s) |
---|---|
On-site Delivery Time |
Onsite Delivery Time Value On-site Delivery Time Unit |
Normal Order Time |
Normal Order Time Value Normal Order Time Unit |
Expedited Order Time |
Expedited Order Time Value Expedited Order Time Unit |
Normal Cost | Normal Cost |
Expedited Cost | Expedited Cost |
Holding Cost Rate |
Holding Cost Rate Holding Cost Unit |
Inventory level range |
Min Inventory Level Max Inventory Level |
Current Holding Level | Current Holding Level |
Spare records can be linked to multiple Spare Application records. For each Spare record in the Spares Analysis report, there can be multiple Application Properties sections. The name of the corresponding Application, which is stored in the Application ID field of each Spare Application record, is displayed at the beginning of each Application Properties section.
Each Application Properties section contains the following grids:
The Populations grid displays information stored in Spare Application Population records. There can be multiple Spare Application Population records linked to each Spare Application record. For each Spare Application Population record, one row exists in the Populations grid.
The following table lists each item in the Populations grid and the corresponding Spare Application Population record field whose data is displayed in the report.
Report Item | Record Field(s) |
---|---|
Population Name |
Name |
Population Size |
Population Size |
Population Age |
Age Age Time Unit |
The Failure Distribution grid displays information that is stored in Distribution records that are linked to the Spare Application record. There can be multiple Distribution records linked to each Spare Application record. For each Distribution record, one row exists in the Failure Distribution grid.
The following table lists each item in the Failure Distribution grid and the corresponding Distribution record field whose data is displayed in the report. The values in the Parameter 1, Parameter 2, and Parameter 3 columns will be different depending on whether the Distribution record is an Exponential, Lognormal, Normal, or Weibull distribution.
Report Item | Family | Record Field(s) |
---|---|---|
Name | Distribution |
Onsite Delivery Time Value On-site Delivery Time Unit |
Distribution Type | Distribution |
Normal Order Time Value Normal Order Time Unit |
Time Unit | Distribution |
Expedited Order Time Value Expedited Order Time Unit |
Parameter 1 |
Exponential Lognormal Normal Weibull |
MTBF Mu Fix Mean Beta |
Parameter 2 |
Lognormal Normal Weibull |
Sigma Fix Standard Deviation Eta Note: If the Distribution Type is Exponential, no value is displayed. |
Parameter 3 |
Lognormal Weibull |
Gamma Gamma Note: If the Distribution Type is Exponential or Normal, no value is displayed. |
The Failure Consequence grid displays information stored in the Spare Application record.
The following table lists each item in the Failure Consequence grid and the corresponding Spare Application record field whose data is displayed in the report.
Report Item | Record Field(s) |
---|---|
Preparation Time |
Preparation Time Value Preparation Time Unit |
Repair Time |
Repair Time Value Repair Time Unit |
Labor Cost |
Repair Labor Cost |
Fixed Lost Production Cost | Fixed Lost Production Cost |
Variable Lost Production Cost Rate |
Variable Lost Production Cost Variable Lost Production Unit |
# of Required Spaces |
Required Spares |
The Preventive Maintenance grid displays information stored in the Spare Application record.
The following table lists each item in the Preventive Maintenance grid and the corresponding Spare Application record field whose data is displayed in the report.
Report Item | Record Field(s) |
---|---|
Time-based Replacement Interval |
PM Interval Value PM Interval Unit |
Labor Cost |
PM Labor Cost |
Downtime |
PM Downtime Value PM Downtime Unit |
If you have run a Monte Carlo simulation, the Spares Analysis graphs will appear in the Spares Analysis report with the results from the last simulation that was run.
Copyright © 2018 General Electric Company. All rights reserved.