The baseline GE Digital APM database includes the Production Analysis Report, which you can use to view a summary of the results of a Production Analysis.
The Production Analysis Report is built from the following Catalog items:
Throughout this documentation, we refer to the main report, the subreport, and the supporting queries collectively as the Production Analysis Report.
The Production Analysis report contains a prompt on the ENTY KEY field in the Production Analysis family. When you run the Production Analysis report via the Production Analysis module, the ENTY KEY of the Production Analysis record associated with the current analysis is passed automatically to the prompt, and the results for the current Production Analysis are displayed. If you run the main report or any of the queries in the preceding list directly from the Catalog, however, you will need to supply the ENTY KEY of a Production Analysis record manually to retrieve results. The subreport (i.e., Catalog item SubreportProductionAnalysis) cannot be run directly from the Catalog.
The Analysis Summary section of the Production Analysis report displays information that is stored in the Production Analysis record.
The following table lists each item in the Analysis Summary section and the corresponding Production Analysis record field whose data is displayed in the report.
Report Item | Production Analysis Field |
---|---|
Analysis Name |
Analysis ID |
Analysis Description |
Short Description |
Start Date |
Analysis Start Date |
End Date | Analysis End Date |
Process Reliability |
Pro Reliability |
Total Data Points |
Total Data Points |
Ignored Data Points | Ignored Data Points |
Min Production | Min Production |
Unit Of Measure | Unit Of Measure |
Margin | Margin Value |
Last Modified | LAST UPDT DT |
Modified By |
LAST UPBY SEUS KEY Note: The name of the Security User associated with this value is displayed in the report. |
The Production Lines section of the Production Analysis report contains a grid that displays information that is stored in the Weibull records that are linked to the Production Analysis record. Each row in the grid represents one Weibull record that is linked to the Production Analysis record.
The following table lists each column in the grid in the Production Lines section and the corresponding Weibull record field whose data is displayed in the report.
Column | Weibull Field |
---|---|
Name |
Analysis ID |
Beta |
Beta |
Eta |
Eta |
R2 | R -Squared |
Goodness of Fit |
Passed |
The Production Regions section of the Production Analysis report contains a grid that displays information that is stored in the Production Losses records that are linked to the Production Analysis record. Each row in the grid represents one Production Losses record that is linked to the Production Analysis record.
The following table lists each column in the grid in the Production Loss Regions section and the corresponding Production Losses record field whose data is displayed in the report.
Column | Production Losses Field |
---|---|
Name |
Losses Type |
Region Start |
Area Start |
Region End |
Area End |
Quantity | Production Losses |
Cost |
Losses Cost |
The Production Weibull Plot section of the Production Analysis report displays the Production Weibull Plot.
The Production Data section of the Production Analysis report contains a grid that displays information that is stored in the Production Data field in the Production Analysis record.
The following columns of information are displayed in the grid in the Production Data section. The values displayed in these columns are stored in the Production Data field in the Production Analysis record:
Copyright © 2018 General Electric Company. All rights reserved.