Steps
In the page heading, select
If the query has already been saved, any changes that you have made will be saved to the same Catalog folder with the existing Catalog item properties. If the query has not yet been saved, the Save As window will appear.
The following instructions assume that you are saving the query for the first time.
Note: If you are viewing a previously saved query and you want to save a copy of the current query with a different name or to a different location, you can select
In the Name box, enter a name for the query. The name is required and must be unique to the Catalog folder in which you are saving the query.
The Caption box is populated automatically with the value that you entered in the Name box.
In the Description box, you can enter a description for the query. This is not required to save the query.
The Of type box is populated automatically with the Catalog item type.
Select Save.
The query is saved to the Catalog.
Copyright © 2018 General Electric Company. All rights reserved.