Policy Event Records

Policy Event records store information about events that are associated with Equipment or Functional Location records that are monitored by a policy. The following table provides an alphabetical list and description of the fields that exist in the Policy Event family and that are displayed on the baseline Policy datasheet (unless otherwise noted). The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Close Description

Text

A description of why the event was closed.

Populated automatically based on the properties defined for the associated Create Event or Close Event node.

Description

Text

A description of the event.

Populated automatically based on the properties defined for the associated Create Event node.

End Time

Date

The date on which the event ended.

Populated automatically based on the properties defined for the associated Create Event or Close Event node.

This field is used only when the Has Duration field is set to True.

Event Type

Character

The type of event.

Populated automatically based on the properties defined for the associated Create Event node.

Has Duration

Logical

Indicates whether or not there is an end time associated with the event.

Populated automatically based on the properties defined for the associated Create Event node.

Name

Character

The name of the event.

Populated automatically based on the properties defined for the associated Create Event node.

In the Execution History pane, this value will appear as a hyperlink that you can select to access the Events section in Asset Health Manager.

Policy Instance GUID

Binary

A unique identifier that is used internally by the GE Digital APM system.

On the Policy Event datasheet, this field is labeled Link to Policy and contains a link to the policy instance that created the Policy Event record.

Severity

Character

The severity of the event.

Populated automatically based on the properties defined for the associated Create Event node.

Start Time

Date

The date on which the event started.

Populated automatically based on the properties defined for the associated Create Event node.

Time Line Reset

Logical

This field is not currently used.

N/A

Copyright © 2018 General Electric Company. All rights reserved.