Field Description of the Schedule Logs Page

The following table lists the fields that are available in the In Progress, Successful, and Failed sections of the Schedule Logs page.

Fields Type Description Behavior and Usage
Description Text

The description that you have provided for the scheduled task.

Populated automatically based on the description that you have provided for a task.

Tip: It is recommended that you provide the name of the task for which you are scheduling an operation.

Download Log N/A The log of the tasks that are completed. You can select the download button () to download the log file for the scheduled tasks that are completed and are in a Successful or Failed state.
Error Details Text The details of the error.

This field appears in the Failed section and is populated automatically.

Percent Complete Number The percentage completion of the scheduled task. This field appears in the In progress section and is populated automatically.
Runtime Number The time taken for the completion of a scheduled task. This field appears in the Successful section and is populated automatically.
Started Date The time at which the schedule process started. Populated automatically based on the schedule defined for the task.
Type Text The type of task that is scheduled.

Populated automatically based on the schedule that you have defined for task.

For example, if you have scheduled a KPI to be updated at a particular time period via the Schedule, Alerts and Privileges section, then the In Progress section displays the type as KPI.

Copyright © 2018 General Electric Company. All rights reserved.