The Schedule Logs page shows the status of the various processes that are scheduled in the GE Digital APM system. The available statuses, In Progress, Successful, and Failed, are tabs on the Schedule Logs page.
The following image shows the Schedule Logs page.
The Schedule Logs page contains the following sections:
In Progress: When the scheduler is running, the job appears in the In Progress section. On completion of the scheduled run process, the result is either Successful or Failed.
Note: At any given time, only 5 scheduled jobs will be running. The other jobs will be in queue.
Failed: If the scheduled job is run and an error occurs, the job appears in the Failed section. This section also displays the error details.
Note: If the scheduler stops due to server failure or shut down, then the schedule status is displayed as Failed.
Copyright © 2018 General Electric Company. All rights reserved.