The following tables outline the steps that you must complete to upgrade this module to
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Step | Task | Notes |
---|---|---|
1 |
Add WHERE criteria to the following queries to accommodate date filters:
|
This step is required only if you have previously modified the queries. You can add the WHERE criteria by following the instructions in KBA 6215. If you have not modified your queries, you do not need to follow this step. This step will be completed automatically when you upgrade the components in the basic GE Digital APM system architecture. |
Step | Task | Notes |
---|---|---|
1 | Revert the My Open Inspections Query to baseline. |
This step is required only if you have previously modified the My Open Inspections query. If you have, you will not have the ability to download inspections from the My Open Inspections section of the Inspections page until you revert the My Open Inspections query to baseline for the offline functionality to be enabled. Note: If you want to modify this query, you must have both the Inspection Lock and the Entity Key fields as selected fields in the customized query.
|
This module will be upgraded to
This module will be upgraded to
This module will be upgraded to
This module will be upgraded to
This module will be upgraded to
Step | Task | Notes |
---|---|---|
1 | This step is optional. |
Step | Task | Notes |
---|---|---|
1 | This step is optional. |
Step | Task | Notes |
---|---|---|
1 | If you have added System Codes to the MI_INSPECTION_TYPE System Code Table, create Task Types records representing those task types, and then set the value in the Reference field to Inspection. | This step is required only if you have added System Codes to the MI_INSPECTION_TYPE System Code table. |
2 | This step is optional. |
Copyright © 2018 General Electric Company. All rights reserved.