The following instructions provide details on upgrading the Process Data Integration Service on the Process Data Integration Server. These instructions assume that you are an Administrator with full access to the Meridium Process Data Integration server machine.
Steps
On the machine that will serve as the Meridium Process Data Integration Server, access the GE Digital APM distribution package, and then navigate to the folder \\Setup\Meridium APM Server and Add-ons.
Select the file setup.exe.
A message appears, asking if you want to allow setup.exe to make changes to your machine.
Select Yes.
The Meridium APM Server and Add-ons installer appears, displaying the Preparing Setup screen. The Preparing Setup screen contains a progress bar that indicates when the installer is ready to upgrade the components on your machine.
When the progress bar reaches the end, a message appears, asking if you want to upgrade your server.
Select Yes.
The Setup Status screen appears, displaying a progress bar that indicates the status of the upgrade process. After the progress bar reaches the end, the Maintenance Complete screen appears.
You can also select to optionally launch the APM System Administration tool when the installer window closes.
Select Finish.
The upgrade is complete.
What's Next?
Copyright © 2018 General Electric Company. All rights reserved.