If you are upgrading from one version of the ABAP service pack add-on to a newer version, you will need to uninstall the currently installed service pack.
Note: The uninstall feature is available only in SAP versions S/4 Hana 1511 and later. To complete these steps, you must use SAP client 000.
Steps
Enter SAINT.
The Add-On Installation Tool screen appears.
Select the Uninstallable components tab.
MIAPM appears in the list of add-on packages that can be uninstalled.
Select MIAPM, and then select Continue.
The Start options dialog box appears.
Select .
The status is updated to indicate that the add-on package will now be imported and the uninstallation process continues. When the process completes, the status is updated to show that the add-on package was removed successfully.
Results
The MIAPM add-on package is removed from the list of installed add-on packages in the Add-On Installation Tool screen.
Copyright © 2018 General Electric Company. All rights reserved.