Deploy Asset Strategy Implementation (ASI) for the First Time

The following table outlines the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic GE Digital APM system architecture.

These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.

Note: This GE Digital APM module is not available in the APM Now environment.

Step Task Notes
1 Install the ASI for SAP ABAP add-on on your SAP System. This step is required.
2 Verify ASI ABAP Add-On. This step is required.
3 Review the ASI data model to determine which relationship definitions you will need to modify to include your custom equipment and location families. Via Configuration Manager, modify the relationship definitions as needed. Required only if you store equipment and location information in families other than the baseline Equipment and Functional Location families.
4 Assign Security Users to one or more of the ASI Security Groups and Roles. This step is required.
5 Configure SAP for external numbering. This step is required.
6 Configure SAP permissions. This step is required.
7 Configure Work Management Item Definition records via the ASI Application Settings. This step is required only if you want to use Work Management Item Definition records beyond those provided with the baseline database.

Related Information

Copyright © 2018 General Electric Company. All rights reserved.