Process Data Integration Server Roles

The following server roles are configured on the Process Data Integration Server in the GE Digital APM test environment.

Note: Roles and features can be added via the Add Roles and Features Wizard on a Windows Server machine. To add roles and features, in Server Manager, on the Manage menu, select Add Roles and Features to open the wizard. Select role-based or feature based installation and then continue through the wizard.

In the Server Roles section:

In the Role Services section for the Application Server:

Copyright © 2018 General Electric Company. All rights reserved.