Note: To deploy translations for Operator Rounds, in addition to completing the following steps, you will also need to ensure that the regional setting on the device is set to the corresponding language.
Steps
On the Windows Start menu, select Programs.
The Programs screen appears.
Select APM Mobile Framework.
The APM Mobile Framework screen appears.
Select Applications.
The Add/Remove Applications screen appears.
In the list of available applications, select the Install button that appears to the right of the application that you want to install.
A message appears, asking if you are sure that you want to install translations for the selected language.
Select Yes.
The installation process begins. APM Mobile Framework closes, and the translations are installed.
Note: After the installation is complete, the APM Mobile Framework will reopen automatically and return you to the APM Mobile Framework screen.
Copyright © 2018 General Electric Company. All rights reserved.