Install the Process Data Integration Service

The following instructions provide details on installing the Process Data Integration Service using the GE Digital APM Server and Add-ons installer.

Steps

  1. On the machine that will serve as the Meridium Process Data Integration Server, access the GE Digital APMM distribution package, and then navigate to the folder \\Setup\Meridium APM Server and Add-ons.

  2. Double-click the file Setup.exe.

    The Welcome screen appears.

  3. Select Next.

    The License Agreement screen appears.

  4. Read the License Agreement and, if you agree, select the I accept the terms of the license agreement check box. Then, select Next.

    The Select Installation Location screen appears.

  5. Select Next to accept the default location.

    The Select the features you want to install screen appears.

  6. Select the Meridium Process Data Integration Service option.

    Note: While additional options are available for selection, these options are not meant to be installed on the Process Data Integration Server. These instructions assume that you want to install only the Meridium Process Data Integration Service software. When this software is installed, the GE Digital APM System Administration Tool will also be installed automatically.

  7. Select Next.

    GE Digital APM performs a check to make sure that your machine contains the required prerequisites for the features that you want to install.

  8. Select Install.

    The Setup Status screen appears, which displays a progress bar that shows the progress of the installation process. After the progress bar reaches the end, a message appears, indicating that your server is being configured. After your server is configured, the Installation is Complete screen appears.

    You can also select to optionally launch the APM System Administration tool when the installer window closes.

  9. Select Finish.

    The installation is complete.

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.