Install Operator Rounds on Windows Mobile Device

Steps

  1. On the Windows Start menu, select Programs.

    The Programs screen appears.

  2. Select APM Mobile Framework.

    The APM Mobile Framework screen appears.

  3. Select Applications.

    The Add/Remove Applications screen appears.

  4. In the list of available applications, select the Install button that appears to the right of Operator Rounds.

    A message appears, asking if you want to install Operator Rounds.

  5. Select Yes.

    The installation process begins. The APM Mobile Framework closes, and the Operator Rounds application is installed.

    Note: After the installation is complete, the APM Mobile Framework will reopen automatically and return you to the APM Mobile Framework screen.

Copyright © 2018 General Electric Company. All rights reserved.