The following tables outline the steps that you must complete to upgrade this module to
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
This module will be updated to
This module will be upgraded to
Step | Task | Notes |
---|---|---|
1 | Modify the application-wide Asset Hierarchy configuration to include the Asset Folder and AMS Asset families. | This step is required only if you are not using Equipment and Functional Location records and want to view AMS Asset Folders and AMS Assets in a hierarchy. |
2 | Configure the message queue section in the Web Service Details section of the AMS Data Source Configuration UI page. | This step is required only if you are using message queues to receive data from an AMS server. |
3 | Run the following update query: UPDATE [MI_APTAG] SET [MI_APTAG].[MI_TAG_SYSTEM_ID_C] = [MI_APTAG].[MI_TAG_PATH_C]. | This step is required only if you want to use the AMS Asset Tag Data Loader to create relationships between tags and assets. |
4 |
After you upgrade your database, use the State Management option in the Revert to Baseline feature to apply the new baseline State Configuration for the AMS Recommendation family. |
This step is required only if you were using State Configuration for the AMS Recommendation family in a version prior to V4.2.0.0. As of V4.2.0.0, the State Configuration for the AMS Asset Recommendation family is enabled and configured to use the parent’s (Performance Recommendation family’s) State Configuration settings. The baseline state configuration must be applied in order for various queries and lists in GE Digital APM to function as expected. |
Step | Task | Notes |
---|---|---|
1 | Modify the application-wide Asset Hierarchy configuration to include the Asset Folder and AMS Asset families. | This step is required only if you are not using Equipment and Functional Location records and want to view AMS Asset Folders and AMS Assets in a hierarchy. |
2 | Configure the message queue section in the Web Service Details section of the AMS Data Source Configuration UI page. | This step is required only if you are using message queues to receive data from an AMS server. |
3 | Run the following update query: UPDATE [MI_APTAG] SET [MI_APTAG].[MI_TAG_SYSTEM_ID_C] = [MI_APTAG].[MI_TAG_PATH_C]. | This step is required only if you want to use the AMS Asset Tag Data Loader to create relationships between tags and assets. |
4 |
After you upgrade your database, use the State Management option in the Revert to Baseline feature to apply the new baseline State Configuration for the AMS Recommendation family. |
This step is required only if you were using State Configuration for the AMS Recommendation family in a version prior to V4.2.0.0. As of V4.2.0.0, the State Configuration for the AMS Asset Recommendation family is enabled and configured to use the parent’s (Performance Recommendation family’s) State Configuration settings. The baseline state configuration must be applied in order for various queries and lists in GE Digital APM to function as expected. |
Step | Task | Notes |
---|---|---|
1 | Modify the application-wide Asset Hierarchy configuration to include the Asset Folder and AMS Asset families. | This step is required only if you are not using Equipment and Functional Location records and want to view AMS Asset Folders and AMS Assets in a hierarchy. |
2 | Configure the message queue section in the Web Service Details section of the AMS Data Source Configuration UI page. | This step is required only if you are using message queues to receive data from an AMS server. |
3 | Run the following update query: UPDATE [MI_APTAG] SET [MI_APTAG].[MI_TAG_SYSTEM_ID_C] = [MI_APTAG].[MI_TAG_PATH_C]. | This step is required only if you want to use the AMS Asset Tag Data Loader to create relationships between tags and assets. |
4 |
After you upgrade your database, use the State Management option in the Revert to Baseline feature to apply the new baseline State Configuration for the AMS Recommendation family. |
This step is required only if you were using State Configuration for the AMS Recommendation family in a version prior to V4.2.0.0. As of V4.2.0.0, the State Configuration for the AMS Asset Recommendation family is enabled and configured to use the parent’s (Performance Recommendation family’s) State Configuration settings. The baseline state configuration must be applied in order for various queries and lists in GE Digital APM to function as expected. |
Step | Task | Notes |
---|---|---|
1 | Modify the application-wide Asset Hierarchy configuration to include the Asset Folder and AMS Asset families. | This step is required only if you are not using Equipment and Functional Location records and want to view AMS Asset Folders and AMS Assets in a hierarchy. |
2 | Configure the message queue section in the Web Service Details section of the AMS Data Source Configuration UI page. | This step is required only if you are using message queues to receive data from an AMS server. |
3 | Run the following update query: UPDATE [MI_APTAG] SET [MI_APTAG].[MI_TAG_SYSTEM_ID_C] = [MI_APTAG].[MI_TAG_PATH_C]. | This step is required only if you want to use the AMS Asset Tag Data Loader to create relationships between tags and assets. |
4 |
After you upgrade your database, use the State Management option in the Revert to Baseline feature to apply the new baseline State Configuration for the AMS Recommendation family. |
This step is required only if you were using State Configuration for the AMS Recommendation family in a version prior to V4.2.0.0. As of V4.2.0.0, the State Configuration for the AMS Asset Recommendation family is enabled and configured to use the parent’s (Performance Recommendation family’s) State Configuration settings. The baseline state configuration must be applied in order for various queries and lists in GE Digital APM to function as expected. |
Step | Task | Notes |
---|---|---|
1 | Modify the application-wide Asset Hierarchy configuration to include the Asset Folder and AMS Asset families. | This step is required only if you are not using Equipment and Functional Location records and want to view AMS Asset Folders and AMS Assets in a hierarchy. |
2 | Configure the message queue section in the Web Service Details section of the AMS Data Source Configuration UI page. | This step is required only if you are using message queues to receive data from an AMS server. |
3 | Run the following update query: UPDATE [MI_APTAG] SET [MI_APTAG].[MI_TAG_SYSTEM_ID_C] = [MI_APTAG].[MI_TAG_PATH_C]. | This step is required only if you want to use the AMS Asset Tag Data Loader to create relationships between tags and assets. |
4 |
After you upgrade your database, use the State Management option in the Revert to Baseline feature to apply the new baseline State Configuration for the AMS Recommendation family. |
This step is required only if you were using State Configuration for the AMS Recommendation family in a version prior to V4.2.0.0. As of V4.2.0.0, the State Configuration for the AMS Asset Recommendation family is enabled and configured to use the parent’s (Performance Recommendation family’s) State Configuration settings. The baseline state configuration must be applied in order for various queries and lists in GE Digital APM to function as expected. |
Step | Task | Notes |
---|---|---|
1 | Modify the application-wide Asset Hierarchy configuration to include the Asset Folder and AMS Asset families. | This step is required only if you are not using Equipment and Functional Location records and want to view AMS Asset Folders and AMS Assets in a hierarchy. |
2 | Configure the message queue section in the Web Service Details section of the AMS Data Source Configuration UI page. | This step is required only if you are using message queues to receive data from an AMS server. |
3 | Run the following update query: UPDATE [MI_APTAG] SET [MI_APTAG].[MI_TAG_SYSTEM_ID_C] = [MI_APTAG].[MI_TAG_PATH_C]. | This step is required only if you want to use the AMS Asset Tag Data Loader to create relationships between tags and assets. |
4 |
After you upgrade your database, use the State Management option in the Revert to Baseline feature to apply the new baseline State Configuration for the AMS Recommendation family. |
This step is required only if you were using State Configuration for the AMS Recommendation family in a version prior to V4.2.0.0. As of V4.2.0.0, the State Configuration for the AMS Asset Recommendation family is enabled and configured to use the parent’s (Performance Recommendation family’s) State Configuration settings. The baseline state configuration must be applied in order for various queries and lists in GE Digital APM to function as expected. |
Step | Task | Notes |
---|---|---|
1 | Modify the application-wide Asset Hierarchy configuration to include the Asset Folder and AMS Asset families. | This step is required only if you are not using Equipment and Functional Location records and want to view AMS Asset Folders and AMS Assets in a hierarchy. |
2 | Configure the message queue section in the Web Service Details section of the AMS Data Source Configuration UI page. | This step is required only if you are using message queues to receive data from an AMS server. |
3 | Run the following update query: UPDATE [MI_APTAG] SET [MI_APTAG].[MI_TAG_SYSTEM_ID_C] = [MI_APTAG].[MI_TAG_PATH_C]. | This step is required only if you want to use the AMS Asset Tag Data Loader to create relationships between tags and assets. |
4 |
After you upgrade your database, use the State Management option in the Revert to Baseline feature to apply the new baseline State Configuration for the AMS Recommendation family. |
This step is required only if you were using State Configuration for the AMS Recommendation family in a version prior to V4.2.0.0. As of V4.2.0.0, the State Configuration for the AMS Asset Recommendation family is enabled and configured to use the parent’s (Performance Recommendation family’s) State Configuration settings. The baseline state configuration must be applied in order for various queries and lists in GE Digital APM to function as expected. |
Step | Task | Notes |
---|---|---|
1 | Modify the application-wide Asset Hierarchy configuration to include the Asset Folder and AMS Asset families. | This step is required only if you are not using Equipment and Functional Location records and want to view AMS Asset Folders and AMS Assets in a hierarchy. |
2 | Configure the message queue section in the Web Service Details section of the AMS Data Source Configuration UI page. | This step is required only if you are using message queues to receive data from an AMS server. |
3 | Run the following update query: UPDATE [MI_APTAG] SET [MI_APTAG].[MI_TAG_SYSTEM_ID_C] = [MI_APTAG].[MI_TAG_PATH_C]. | This step is required only if you want to use the AMS Asset Tag Data Loader to create relationships between tags and assets. |
4 |
After you upgrade your database, use the State Management option in the Revert to Baseline feature to apply the new baseline State Configuration for the AMS Recommendation family. |
This step is required only if you were using State Configuration for the AMS Recommendation family in a version prior to V4.2.0.0. As of V4.2.0.0, the State Configuration for the AMS Asset Recommendation family is enabled and configured to use the parent’s (Performance Recommendation family’s) State Configuration settings. The baseline state configuration must be applied in order for various queries and lists in GE Digital APMM to function as expected. |
Copyright © 2018 General Electric Company. All rights reserved.