During proof testing, if you observe an abnormality or failure that cannot be resolved immediately, you can create a Recommendation. You can also attach an image to the recommendation.
Note: You can create Recommendations for a Proof Test only if the Proof Test is executed using the Mobile Proof Testing module.
Steps
On the upper-right corner of the page, select
The Recommended Actions pane appears, displaying a list of Recommendations that are associated with the Proof Test.
A blank datasheet for the Recommendation appears.
As needed, enter values in the available fields.
On the upper-right corner of the datasheet, select
The Recommendation for the Proof Test is created.
Results
If there are two Proof Tests for the same Instrumented Function, then the Recommendation will appear in the list of Recommendations for both the Proof Tests.
Copyright © 2018 General Electric Company. All rights reserved.