Map Query Workflow

This workflow provides the basic, high-level steps for using this module. The steps and links in this workflow do not reference every possible procedure. For more procedures, see the links in the Related Information section.

  1. Use the GIS Data Loader to load your geospatial data into GE Digital APM
  2. Modify the Baseline Map Query

The baseline Map query is highly customizable, and more complex queries can be created using the following additional steps:

  1. Create criteria
  2. Create prompts
  3. Create hyperlinks

You can also use the following type of SQL query to further customize your map and the data displayed on it.

Copyright © 2018 General Electric Company. All rights reserved.