MI MOC Checklist Records

MI MOC Checklist records store information about Checklists associated with Change Projects. The MI MOC Checklist family is also used to store information about the Checklists that you created using the Application Settings for MOC. This topic provides an alphabetical list and description of the fields that exist for the MI MOC Checklist family and appear on the MI MOC Checklist datasheet. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Checklist ID Character The identification for the Checklist.

This field is automatically populated with a unique value.

Description Character The description of the Checklist. This field is populated with the value in the Description field of the MI MOC Checklist record whose copy is being created.
Is Admin Setting Boolean Indicates whether the Checklist represents a record created in the Application Setting.

This field does not appear on the datasheet.

This field is True if you created the record using the Application Settings for MOC.

This field is False if GE Digital APM automatically created the record as a copy of the Checklist that you created.

Copyright © 2018 General Electric Company. All rights reserved.