When a change is being implemented, it directly or indirectly has an impact on other families in GE Digital APM. In MOC, you can associate a Change Project with records from other families in GE Digital APM that are possibly impacted by the change. Such records are called Changed Elements.
For example, when the change involves replacing the existing pressure relief devices that were identified as Independent Protection Layers, with a different manufacturer's device, the LOPA assessment with which the equipment is associated may be impacted. In this case, the affected LOPA record is a changed element and you can associate the LOPA record with the Change Project.
Changed elements help keep track of all affected processes and records in one place, which you can then analyze to assess the advantages and disadvantages of implementing the change. An approver can review the changed elements to understand the impact of the change and make decisions on whether to approve or request rework of the Change Project. Changed elements provide your organization with a means of associating impacted areas as changed elements, thus making MOC a fully auditable tool.
Copyright © 2018 General Electric Company. All rights reserved.