Link a LOPA to a Consequence

This topic describes how to link a LOPA to a Consequence in Hazards Analysis.

Note: You can create or link a LOPA to a Consequence only if the associated Hazards Analysis is in the Planning State.

Steps

  1. Access the System/Node that is linked to the Consequence that you want to access.
  2. Select the Hazards Worksheets tab.

    The Hazards Worksheets section appears, displaying a hierarchical view of the components (Deviations or What Ifs, Causes, Consequences, and Safeguards) associated with the System/Node.

    Hazards Worksheet

  3. Select the Consequence to which you want to link the LOPA.

    Select Consequence to Link or Create LOPA

  4. In the Consequence that you selected, select Link.

    Note: If a Consequence is already linked to a LOPA, the link Unlink will appear. You can either select another Consequence, or unlink the LOPA from the Consequence, and then link to a different LOPA.

    The LOPA window appears, displaying a list of LOPA that belong to the same site as that assigned to the Hazards Analysis.

    LOPA Window

  5. Select the row containing the LOPA that you want to link to the Consequence.

  6. Select Link.

    The LOPA is linked to the Consequence.

    Consequence Linked With LOPA

Results

Copyright © 2018 General Electric Company. All rights reserved.