About Events with Only One Cause

Some types of events have only one possible cause. In Events where the value in Capacity Event Type field identifies a single-cause event, the Cause Code System, Cause code Component, and Cause Code fields will be disabled and populated automatically with the appropriate cause code. The following table lists these Capacity Event Type values and their corresponding Cause Code values.

Capacity Event Type Cause Code System Cause Code Component Cause Code
IR (Inactive Reserve) Inactive State Inactive State 0002 (Inactive Reserve)
MB (Mothballed) Inactive State Inactive State 9991 (Mothballed Unit)
RS (Reserve Shutdown) External Economic 0000 (Reserve Shutdown)
RU (Retired) Inactive State Inactive State 9990 (Retired Unit)

Copyright © 2018 General Electric Company. All rights reserved.