Export Metadata

For exporting GE Digital APM metadata, you can choose the items of each supported data type and any combination of any data types you wish to export. However, large exports can take a considerable amount of time.

Steps

  1. Access the Export page.

  2. In the Available Items section, perform the following steps:
    1. Select the data type (such as Families, Filters and Fields, Family Rules and so on) from the Select metadata type drop-down list.

      All the metadata in that data type appears in the Available Items section.

    2. If you want to export all the metadata in the selected data type, select Move all the metadata.

      -or-

      If you want to export only some of the metadata in a data type, select the check box for metadata that you want to export and then select Move selected metadata .

      All the selected metadata that you chose to export appear in Selected Items section.

      Hint: You can also search for metadata in a data type (by name) by selecting .

      Note: If you want to remove the selections from the Selected Items list, then select the check box for the items, and then select Remove the selected item. The metadata removed from the Selected Items list will be available for selection in the Available Items section.

  3. In the File Name box, provide the name of the file, and then select the file type from the File Type box.

    Note: By default, the Include underlying Query/Dataset/Subreports check box is selected. If you do not want to export the underlying queries or datasets, then clear the Include underlying Query/Dataset/Subreports check box.

  4. Select Start Export.

Result

Copyright © 2018 General Electric Company. All rights reserved.