You can configure a field to contain a list of System Codes defined in a System Code Table. When you create a Valid Values list in this way, the drop-down list of valid values will display any System Codes that are defined in the specified System Code table. The list will be updated automatically to reflect changes made to the System Code table. The Valid Values list created by the using the Behaviors section is restricted (i.e., the users will only be allowed to select from the values that are displayed in the list). They will not be able to enter their own values in the list.
Note: Only active System Codes that are constructed via System Codes and Tables feature will appear in valid values lists.
Steps
In the Fields section, select
The workspace for the selected field appears, displaying the Information section.
As needed, enter values in the available fields.
Select the Behavior tab, and then in the Valid Value box, select System code and Table.
The Select Valid Values System Code Table box appears.
In the Select Valid Values System Code Table box, select the System Code Table from which you want to build the list of valid values.
The list of the filter types appear.
If you want the list of valid values to include all of the System Codes in the selected System Code table, select the No Filter check box.
Note: If the System Code table that you selected in the previous step does not contain any references, only the No Filter option is available.
-or-
If you want the list of valid values to contain only the System Codes that are referenced from a System Code in another System Code table, then select the Static Filter check box.
The Choose System Code Table and Choose System Code boxes appears.
In the Choose System Code Table box, select the System Code table that will be used as the filter.
The list of System Codes appears in the Choose System Code table.
In the Choose System Code box, select the required System Code.
Note: The list will contain only the System Codes from the source System Code table that are referenced by the System Code that you select here.
Select
A list of valid values is created.
Copyright © 2018 General Electric Company. All rights reserved.