Add a System Code Table

Steps

  1. Access the System Codes and Tables page.
  2. In the System Tables section, select .

    An empty form appears in the Add Table section.

  3. In the ID box, enter the System Code Table ID.

    Note: This is a required field. The ID must be unique and must not exceed 50 characters.

  4. In the Description box, enter a description for the table.

    Note: This description should specify the purpose of the table and the type of codes present within the table. The description must be limited to 255 characters. The description that you provide appears as table name in the System Code and Tables section.

  5. In the Display Format subsection, select a display format that specifies how the codes will be displayed.

    You can select one of the following options:

    Note: If you choose Code Only, your code must be descriptive.

  6. Select .

    The new System Code Table is created and added to the list of all System Code Tables.

Copyright © 2018 General Electric Company. All rights reserved.