Add References to the System Code

Steps

  1. Access the System Codes and Tables page.
  2. In the System Tables section, select the System Code Table that contains the System Code to which you want to add a reference.

    The properties of the table appear.

  3. In the System Code subsection, select the System Code for which you want to add a reference.

    The References subsection appears.

  4. In the References subsection, select .

    The Add System Code as Reference window appears, displaying the list of references.

    Add System Code as Reference window

  5. Select the check box for each reference that you want to add.
  6. Select Add.

    The selected references are added and appear in the list of references for the System Code in the References subsection.

Copyright © 2018 General Electric Company. All rights reserved.