Steps
If, on the upper-left corner of the page, the <number> Error link appears beside the
Note: If the number of errors link does not appear, then the connections needed to use the data loaders are configured properly.
The Connection Errors dialog box appears displaying the connections status for each connection point needed to use the data loaders.
Select OK.
The connection status is tested.
Results
The following table describes the connection status for data import jobs.
Connection Test | Description | If you get an Error... |
---|---|---|
APM Connect Web API Test | Test the connection between the GE Digital APM web API and the APM Connect server. | Ensure the ports are open between the GE Digital APM Server and the APM Connect server. |
APM Connect Configuration Test | Test the configuration of the APM Connect connection parameters configured in GE Digital APM. |
Ensure the parameters configured in GE Digital APM are correct to establish connection from GE Digital APM and APM Connect. |
APM Fileshare Access Test | Tests the file share system is connected to the GE Digital APM Server, so that the server can read and write to the configured file shares. |
Ensure the parameters configured in GE Digital APM are correct to establish connection from GE Digital APM, and the user has the necessary permissions to access the file share. |
APM Staging Database Test | Tests the GE Digital APM Server is connected tot the APM Connect IR database. | Ensure that PostgresSQL is accepting the connection from GE Digital APM . These connections are managed in the file pg_hba.conf. |
APM Connect Fileshare Access Test | Tests the file share system is connected to the APM Connect server, so that the server can read and write to the configured file shares. |
Ensure the parameters configured in GE Digital APM are correct to establish connection from GE Digital APM, and the user has the necessary permissions to access the file share. |
APM Connect Staging Database Test | Tests the connection between the APM Connect server and the IR database to ensure that files can read and written to the IR. | Ensure the RunDataLoaderRoute.cfg is configured correctly. |
Copyright © 2018 General Electric Company. All rights reserved.