Classified Equipment Standard Records

Classified Equipment Standard records store classified data produced by a Cognitive Analytics cognition that has processed historic equipment data. This topic provides an alphabetical list and description of the fields that exist for the Classified Equipment Standard family. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Area

Character

The boundaries within a site or plant that describe where the equipment is located.

You can use this field to store classified data produced by a cognition.

Business

Character

If applicable, the name of the business within the company. You can use this field to store classified data produced by a cognition.

Classification Cognition

Character

When this record was last processed, the name of the cognition that was executed.

You can use a Constant node to populate this field.

Classification Date Date When this record was last processed, the date on which the cognition was executed. You can use the Now() function in a Constant node to populate this field.
Classification User Character When this record was last processed, the user who initiated the execution of the cognition. You can use the User() function in a Constant node to populate this field.
Company

Character

The company name within the corporation. You can use this field to store classified data produced by a cognition.
Corporation

Character

The corporation name. You can use this field to store classified data produced by a cognition.
Corporation

Character

A field that indicates how important the piece of equipment is to production. You can use this field to store classified data produced by a cognition.
Equipment Category

Character

The category of equipment, such as:
  • Fixed
  • Rotating
  • Electrical
  • Instruments
You can use this field to store classified data produced by a cognition.
Equipment Class

Character

An equipment class within the equipment category. For example, equipment classes under the Rotating equipment category might be Compressor, Pump, and Engine. You can use this field to store classified data produced by a cognition.
Equipment ID

Character

A unique value that identifies each individual piece of equipment. You can use this field to store classified data produced by a cognition.
Equipment Type

Character

The equipment type within the equipment class. For example, an equipment type under the Pump equipment class is Centrifugal. You can use this field to store classified data produced by a cognition.
Functional Location ID

Character

The physical location of the equipment. You can use this field to store classified data produced by a cognition.
Installation Date Date The installation date of the equipment. You can use this field to store classified data produced by a cognition.
Latitude

Numeric

A numeric value representing the latitudinal position of the equipment.

You can use this field to store classified data produced by a cognition.

IMPORTANT: Values are stored as decimal degrees.

Longitude Numeric The numeric value representing the longitudinal position of the equipment.

You can use this field to store classified data produced by a cognition.

IMPORTANT Values are stored as decimal degrees.

Manufacturer Character The name of the equipment manufacturer. You can use this field to store classified data produced by a cognition.
Model Number Character The model number assigned to the equipment by the manufacturer. You can use this field to store classified data produced by a cognition.
Region Character The geographic region in which the equipment is located. You can use this field to store classified data produced by a cognition.
Short Description

Character

A brief description of the equipment. You can use this field to store classified data produced by a cognition.
Site

Character

The name of the plant or site in which the equipment is located. You can use this field to store classified data produced by a cognition.
Status

Character

The availability of the equipment. You can use this field to store classified data produced by a cognition.
Technical ID

Character

The technical number of the equipment. You can use this field to store classified data produced by a cognition.
Unit

Character

The process location of the equipment within an area in a site or plant. You can use this field to store classified data produced by a cognition.
Unit Type

Character

The type of the material processed within a unit. You can use this field to store classified data produced by a cognition.

Copyright © 2018 General Electric Company. All rights reserved.