Add a User with Permissions

The following instructions can be used to grant existing users permissions to a Public folder in the Catalog.

Note: No user can modify permissions to the Personal or Baseline folder.

Steps

  1. Access the Catalog page.
  2. In the left pane, select the folder whose permissions that you want to modify.

    The workspace for the selected folder appears.

  3. In the workspace heading, select , and then select Folder properties.

    The Catalog Folder Properties window appears, displaying the properties for the selected Catalog folder.

  4. Select Permissions.

    The Permissions section of the Catalog Folder Properties window appears, displaying a grid that contains users and groups that have permissions to create, view, edit, or delete items within the selected folder.

  1. In the upper-right corner of the window, select .

    The User Browser window appears.

  2. Select a user from the list, and then select Done.

    The selected user appears in the grid in the Permissions section of the Catalog Folder Properties window.

  3. As needed, modify the available options to determine the permissions for the user.
  4. Select Done.

    The selected user is granted permissions to the folder.

Copyright © 2018 General Electric Company. All rights reserved.